Other Parts Discussed in Thread: TIDA-00653, UCD3138FW-BIDI
Hi,
I'm having trouble interfacing the TIDA-00653 with Fusion Studio Online. The device is loaded with the provided firmware ().
by using UCD3xxx Device GUI, i was able to download the above firmware onto the device, as well as using Memory Debugger and Bi-DCDC GUI. The Fusion Studio Online detected the device, but returned the error
There was an error bootstrapping the Fusion GUI for the DC-DC @ Address 88d:
The following PMBus commands could not be read from the DC-DC @ Address 88d:VOUT_MODEThese commands are required for Fusion Digital Power Studio to run.Please verify firmware and power and try again or contact customer support if you continue to have difficulties. at TIDP.PMBus.PMBusUIUtils.Verify_Parameters_Readable(PMBusDevice device, IEnumerable`1 command_ids) at TIDP.PMBus.PMBusUIUtils.Verify_Required_Parameters_Readable(PMBusDevice device) at TIDP.WinForms.Apps.DPGUI.DeviceControl.t() at TIDP.WinForms.Apps.DPGUI.DeviceControl.z()
The Fusion GUI can not continue due to this error.
I tried the solution found at but it did not fix the issue.
using Device Debug Report return
Expected X0 File------------None Supplied
Expected Project File-------None Supplied
GUI-------------------------Texas Instruments Fusion Digital Power Studio v3.0.30 [2018-03-02]
SAA-------------------------USB Adapter v1.0.13 [PEC; 400 kHz]
Found program---------------Yes
Device Boots ---------------ToProgram
WARNING---------------------Unknown DEVICE_ID found
I2C Address-----------------88d 0x58
DEVICE_ID-------------------UCD310128V1|0.0.35.0068|120227
[0x55434433313031323856317C302E302E33352E303036387C31323032323700]
MFR_MODEL BidirectionDCDC--[0x4269646972656374696F6E4443444300]
MFR_REVISION----------------E3[0x453300]
MFR_SERIAL------------------XXXXX[0x585858585800]
MFR_ID----------------------TI[0x544900]
MFR_DATE--------------------YYMMDD[0x59594D4D444400]
MFR_LOCATION----------------Dallas, TX[0x44616C6C61732C20545800]
ERROR-----------------------ROM could not be detected after program was sent ENABLE_ROM command
Summary---------------------There is a problem with the device:
Could not access ROM
What do you think would be the solution to this issue?
Thanks,