• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » /etc... Power » /etc... Power Forum » TPS28225 reducing the rise and fall times?
Share
/etc... Power
  • Forum
  • E2E Wiki
Options
  • Subscribe via RSS

Forums

TPS28225 reducing the rise and fall times?

This question is answered
Martin Stübiger
Posted by Martin Stübiger
on Jul 10 2009 06:10 AM
Prodigy30 points

Hello,

I use the Halfbridge driver TPS28225 to drive tow Mosfets from Fairchild (FDS6612A) at a Frequency of 2MHz. Because the fast rise and fall times I have some problems with oscillation at freqencies around 160Mhz. So it is not posible to get the halfbridge to work at 24V bridge voltage because the FET's get quite hot.

After some tests with damping the oscillation of the halfbridge output I wanted to have a try with reducing the rise and fall times by putting a resistance between driver output and gate of the MOSFETs.

My question is now, can I get problems whith the "Dead-Time Control" of the TPS28225 if I do this?

 

Thanks for the help

Power Supply voltage ringing TPS28225
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • nancy!
    Posted by nancy!
    on Jul 15 2009 16:34 PM
    Verified Answer
    Verified by Martin Stübiger
    Intellectual2765 points

    I wanted to have a try with reducing the rise and fall times by putting a resistance between driver output and gate of the MOSFETs.

    Adding resistance in series with the gate-drivers will not reduce the rise and fall times.  Adding resistance in series with the MOSFETs will increase the rise and fall-times by increasing the series resistance and reduce the available current to drive the MOSFET gate charges.  Typically, reducing rise and fall times will make oscillations worse as faster transients are forced on circuit parasitics.

    Adding resistance to increase rise and fall times (reduce slew rates) may reduce the oscillations.  Typically resistance is added in series with the bootstrap capacitor powering the high-side (floating) driver.  This increases the pull-up resistance of the drive and thus slows the rising edge.  This will not impact the dead-time control circuit and should reduce any ringing on the leading edge of the switching node.

     My question is now, can I get problems whith the "Dead-Time Control" of the TPS28225 if I do this?  

    Adding even small resistances in series with the gate drives can adversely affect the dead-time control.  Since dead-time control is monitoring the gate drive voltages at the gate-drive output pins, adding series resistance will cause the driver to sense that the external MOSFET is "OFF" before the MOSFET has actually turned off.  This is why the resistor in series with the bootstrap capacitor is prefered.

    Do not add a resistor in series with the VDD pin to attempt to slow the low-side FET driver as this will cause increased ripple inside the IC and could interfer with the input threshold and logic circuitry.

    If you truly want to reduce the rise / fall times, you will need to select MOSFETs with smaller gate charges, but this will likely increasing ringing rather than decrease it.

    There is a diode based clamping circuit that uses a small (0.1uF) capacitor as close to the MOSFETs Drain/Source (Drain of high-side Source of low-side) and a pair of diodes from SW to the drain of the high-side and from the source of the low-side to the SW pin that can help clamp switching node ringing.  This only slightly reduces the amplitude but does greatly improve the duration of the rining.  To be effective the path inductance must be kept extremely low so very small devices need to be used with very tight layouts.

    It is not the strongest of the species that survives, nor the most intelligent that survives.  It is the one that is the most adaptable to change. - Charles Darwin

    TPS28225
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Martin Stübiger
    Posted by Martin Stübiger
    on Jul 16 2009 03:56 AM
    Prodigy30 points

    Hello Nancy,

    thank you for your helpful recommendations. I did not try them at the moment but I'm shure  they will work out.

    Just some Questions to your recommendations.

    1. Do you mean a circuit like this?

    2. what kind of diodes do you recommend? Shotkey diodes for higher Currents?

     

    Thanks for your help again, Martin

    P.S.: Off course with adding the resistance I wanted to increase the rise time of the driver ;-)

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • nancy!
    Posted by nancy!
    on Jul 16 2009 15:11 PM
    Intellectual2765 points

    Hi Martin,

    Yes, that is the circuit configuration, but what is critical in the loop inductance.  The TPS28225's dead-times are short enough that the ground to SW diode shouldn't carry much average current (less than 2 25ns pulses per switching cycle) and the high-side diode will only carry the ringing energy.  Typically, smaller packaged small signal diodes provide better clamping due to there faster response time.  The low-side diode may need to be slightly larger since it may carry the full load current for a few nano-seconds each switching cycle.

    I can not stress enough that it is layout that is critical.  The goal is to provide a very low impedance path to clamp the switch node ringing.  This means using small packages and very tight layout practices, avoiding vias if possible.  If you have to use vias to make the connection due to board contraints, use 2 vias in parallel to minimize inductance.

    Regards,

    nancy!

    It is not the strongest of the species that survives, nor the most intelligent that survives.  It is the one that is the most adaptable to change. - Charles Darwin

    TPS28225
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use