Welcome to the /etc... Power Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
I am new in field of electronics , my job is to design 100 mAmp constant current source. I find the Texas Ic LM5019 . Plz suggest me this is suitable or there is another model which i can use.
What input voltage?
If you're under 37V I suggest a LM317 coupled as a constant current source. It's cheap and quick.
Iout = Vref / R ==> 0,1 = 1,25/R ==> R = 12.5 Ohm.Power dessipated in the resistor is 0,13W. (Use at least a size SMD 1206 resistor (250mW) for the power loss in resistor)Page 18: http://www.ti.com/lit/ds/symlink/lm117.pdf
Figure: 906316.
Dear Sir
Thanks for your reply
My input voltage is 5V (output of 7805). I have one more problem previously i design this constant source with using 47 ohm 1W resistor ,100 ohm POT and L7805CV voltage regulator . problem is that L7805cv is too hot also resistance
What was your input of the 7805?