B.H.
Hello,
Refers to PMP8251 Schematic -
Whther can I use TPS54325PWP instead of TPS74201RGW to creates 1.5V supply ?
Best regards,
Roie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Roie,
From the TPS54325 product page, it states that "The output voltage can be programmed between 0.76 V and 5.5 V."
You should be able to use it instead of the TPS74201. There will be a loss of specific features (LDO and SoftStart) that may or may not affect the performance of the device you are connecting to. But just in terms of can it provide a 1.5V output, the answer would be yes.
Thanks,