Hi,
i would like to find out how most modern gadgets (smartphone, etc) implement their soft power switch. in iPhone for example, has a tactile power button that turns the device on and off. what IC's and circuitry are involved for such a device to implement this?
in the past, i have implemented such a circuit by controlling the EN pin of a regulator via either a tactile switch or MCU GPIO. i.e. when the device was totally OFF, the EN pin was low and hence power to the system was killed. when the user pressed a tactile button, the EN pin would get pulled up to power the system and the MCU will then hold the EN pin high with a GPIO so that when the user releases the tactile button, the system would still be powered.
I was wondering how most consumer electronics devices commonly implement such soft power witches and what TI IC's might be a good choice.
thanks in advance