This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Load detection

Hello

I am designing an external battery pack that provides 2 dc outputs of 12V@2A(max) and 5V@500mA(max) for my applications. I am using Li ion batteries and DC/DC converters to get the desired voltage levels. I wanted to know if there is any TI IC that could detect an external load connected to my external battery pack? This way I could control the battery drain only when an external load is connected.

Thank You

Shravan