Hi,
I'm trying to make a scap charger with the SM72445, but it seems my duty cycle is being limited when operating in Boost mode. It looks like the limit is about 15%.
I'm not using I2C, so my setting are the following:
A0 = 5V - I'm using the SM72295 to limit the output voltage
A2 = 2.19V - Use H-bridge for PM mode
A4 = 5V - Current limit disabled
A6 = 5V - This is where I have some questions... I want my Iout_th to be 0A. In other words, I want my circuit to ALWAYS enter MPPT mode, because sometimes my load will be 0A, but I need the Vout to be at the value that I set.
Some additional informations:
- The voltage at the VOUT pin on my SM72445 is far from reaching the 5V. Around 3.4V;
- The PV module have a MPPT voltage of 17V, and the voltage at the AVIN pin is set to be 4V when PV is 21V;
- The current sense gain is set to 1V/A, and the highest current that my PV can achieve is 1.2A;
- The reset pint is always high.
If anyone can help me, please do. I'm getting desperate!
If more information is needed, please ask.
Thanks!