Hi, this is Choo.
I have a few questions about 'SM72442(MPPT controller) and AN-2124 SM3320'.
http://www.ti.com/lit/ds/symlink/sm72442.pdf
http://www.ti.com/lit/an/snosb84c/snosb84c.pdf
First of all, my plan is :
Vmpp of my PV panel(Vin of DC/DC converter) : 20~30[V]
Vout of DC/DC converter : about 90[V]
Question 1.
Is it possible to increase a 20~30[V] Vin(Vmpp:supply) to about 90[V] output voltage using 'SM72442(MPPT controller)'?
Question 2.
If my purpose(project) is possible, Please let me know if the 'SM72442' IC is operated as a boost converter or not.
( I want to operate the 'SM72442' IC as only boost converter not buck converter.)
Question3.
Is the temperature sensor(SM72480) essential?
Question4.
I have a serious doubt of whether the microcontoller circuit is essential for proper working of the 'SM72442'
Question5.
If it is impossible to increase a input voltage of 20~30[V] to a output voltage of 90[V] using the 'SM72442', Can you tell me another ICs suitable for my project?
Hope your generous understanding on my mistakes on grammar.
Regards,
Choo.