Hello, all
Now we have one inquiry regarding suit regulator solution from our customer.
Please refer to the item below, and feedback us with your comment.
We are looking for replaceable solution against ADR4533.
LM4132AMF-3.3 seems to be fine, however this maximum input voltage range is less than our expectation.
The required spec for the device is as below;
Vin(max) = 8V
Vout = 3.3V
Initial accuracy = 0.05%@25 degc
Please let us clarify whether you could recommend any other device which supports the specification above.
We thank you in advance for your information.
Best regards,