http://www.ti.com/lit/ds/symlink/sm72442.pdf
Q1)
: According to the SM72442’s Datasheet(page 8.), When the voltage on AVOUT (pin 17) equals the voltage on A0 (pin 14), then the output voltage is maximum output voltage. I want to know whether the output voltage is continuously controlled to the maximum output voltage or the reset pin is pulled low internally After the voltage on AVOUT (pin 17) equals the voltage on A0 (pin 14).
For example, I have designed the following contents
"the voltage on AVOUT (pin 17) equals the voltage on A0 (pin 14) when the output voltage is 90[V]"
If the output voltage reaches 90[V], I want to know whether the SM72442 reset pin is pulled low internally or the output voltage is continuously controlled to 90[V]
Q2)
: According to the SM72442’s Datasheet(page 8.), Overcurrent at the output is detected When the voltage on AIOUT (pin 21) equals the voltage on A4(pin 18). When overcurrent at the output is detected, I want to know the result of detecting the overcurrent. In particular, I’d like to know whether the reset pin is pulled low when overcurrent at the output is detected.
Hope your generous understanding on my mistakes on grammar.