Hi,
I wonder if I can get an answer for the subject-
In my circuit for an ear tag application (small PCB 33x37mm) I'm using MCU, CC1121 and additional sensors- MEMS (ADXL362) and Gyro (LSM6DS3).
I want to add REGULATOR to the circuit. which one should I use? I tested the TP62740 but I'm still thinking of an LDO. in addition, for some reason I'm getting 0.1% of crc errors for the packets i'm sending (not happening when I'm transmitting when connected straight from the battery)..
I'm using an Li-MnO2 battery (3.1v) and I want to regulate 2.2v.
Any advice?
Thanks in advance.