Hi,
I am looking for a switch which can pass frequency higher than 100 kHz and can endure 150 Vpp and 1 A power. It should be driveable with TTL signals. Thanks!
jQ
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
jQ,
I apologize for the multiple redirects.
The signal switches we have in this forum only go up to 0.5 A. I will move this thread to the load switch team which has switches can cover 1A currents.
Thank you,
Adam
Hi jQ,
Looks like you ended up back at the load switch forum. As I mentioned before, we do not have any devices which are suitable here since we do not support voltages that high. I will redirect you to the etc/ forum and see if anyone has the appropriate device.
Thanks,
Alek Kaknevicius