Hi, i have doubts in LM317T Three-Terminal Adjustable Regulator, can someone provide the dropout voltage versus load current curve or data.
regards Siddharth
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Siddharth,
I am not familiar with LM317T, are you referring to one of the following:
LM317, LM317A, LM317-N, LM317M, LM317L.
Attached you will find typical data for the LM317 over current (up to 1A) and temperature. Please note this is not a guarantee of performance but just a typical spec measured on one device.
Best,
Michael
Siddharth,
The dropout voltage curve only shows the difference between Vout and Vin at the point where Vout differs by more than 100mV from the set value. This could be for any Vout (since Vin is in reference to the Vout) within the allowed range of the part. There are various load currents shown across temp but I can get a specific test case in the lab if you can let me know what you need. Do you have a specific output voltage at a specific temp and output current that you would like to see?
Siddharth,
I have attached the Input - Output voltage differential at which the output voltage varied from the set output voltage more than 100mV for a load current 0A to 1.5A. After 1.5A, the part heats up rather quickly making the dropout voltage hard to measure as the device begins to shut down. The datasheet says this is a 1.5A part but in the EC table shows the typical current limit to be 2.2A for the TO-3 package. I would recommend using a heat sink to operate this part above 1.5A.
Let me know if this data is what you need or if you need anything else!
Hi Michael, the most recent curve that you sent shows an input-output deviation of 1.5v at no load or IL=0 amp, which appears to be not matching the low deviation% given in the attached curve from datasheet. Even at 0.5A load the deviation is very low as compared to the curve sent recently , kindly advise
thanks for the details, can you please let me know what is values for VIN, OUT, R1,R2 used to arrive at this curve. regards
Siddharth,
R1 is a 5% 240 ohm and R2 is a 5% 750 ohm. This produces an output voltage of approx. 5.19V but I was measuring around 5.22V during operation. The Vin voltage started several volts above the output voltage (like Vin=8V) and then I decreased Vin until the output voltage dropped by 100mV. So I decreased the input voltage until I measured approx. 5.12V and then recorded that input voltage as the drop out voltage for that specific load current. Then I repeated from a load current from 0A to 1.5A. I also have a 0.1uF input cap and 1uF output cap which is recommended in the datasheet. The purpose of this test is to show how low the input voltage can be in relation to the output voltage for the part to still regulate (regulate within 100mV of the set output voltage).
Thanks for the reply. I hope you mean that for every load current value in the plot the Vout is 5.12v and corresponding Vin can be obtained by adding 5.12v to dropout voltage given in the curve, is this correct?
regards
Siddharth,
Please start a new E2E post for your question regarding the LP3878-ADJ.
Best,
Michael