Hi Team,
I got an inquiry from one of my customers looking for a series voltage reference to replace the MAX6043AAUT33#TG16
Below are the critical parameters:
Temperature stability – 15ppm/C
Initial Accuracy – 0.06%
Supply voltage – 12 V or higher
Low Noise: 4uVp-p at 2.5V output
Operating temp - -40 to 125C
I did try to look for a voltage reference solution similar to the maxim part but it seems like I can't find a solution with greater than 12 V Vin and with low temperature coefficient and low noise.
Please do let me know if I have missed one or if we do have anything in the roadmap.
Thanks!
Regards,
Alfred