I have an design with LM431. It seems have oscillation which burn off the current limiting resistor R1 (1/16W). Please take a look at the schematic to see anything wrong with it...
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Liang,
How long does the system stay up before the resistor burns up?
Do you see 5V at the output as expected? Have you probed the voltage directly from the LM431 device? Looking at the Darlington NPN you selected, it looks like the base voltage will have to be about 1.25V higher than the emitter voltage, which would make the device output about 6.25V. What are the base and emitter voltages?
Chris
Yes, the 5V output was OK.
We never see this problem in house. There were three units return from field with the burn resistor.
Do you want call me instead of time consuming talk like this? My number is 978-268-3292, located in Boston area.
Liang,
See the images I have embedded and also please see the attached TINA schematic file. I have done my best to re-create your schematic. It uses the TL431 instead of LM431 based on model availability, but these parts are similar. Download TI TINA from this link
The results are also embedded in the schematic.
This is a plot of several values vs Rload. You can see as the load decreases the shunt current (blue) increases. I understand this plot shows it goes to 12mA, but this is something you definitely need to confirm in the lab. What is the shunt current as the load goes to zero? If that current gets to 25mA you will have a power dissipation problem in R1. Something else I noticed was the relationship between shunt current and R2. You may want to play with that value as well. That figure is inside the schematic.
Chris