Hi all
Would you mind if we ask TL431?
<Question1>
On the datasheet P16, does "unstable" mean that there is no enought phase margin?
<Question2>
In relation to <Question1>, do you have the blod plot data?
Kind regards,
Hirotaka Matsumoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Matsumoto-san,
1. You are correct, unstable means that there is not enough phase margin. The boundary denotes 0 or close to 0 phase margin.
2. We do not have the bode plots available, however, because the boundary is 0 phase margin, we typically recommend designing at least 1 decade away from the boundary to be stable across temperature and process.
Additionally, please refer to the following application note for additional details. This app note also provides a graph showing where the stability has 30degrees of phase margin to help design.
http://www.ti.com/lit/an/slva482a/slva482a.pdf
Best,
Michael
Michael san
Thank you for your reply always!
We have some additional questions as follows;
<Additional question1>
"This app note also provides a graph showing where the stability has 30degrees of phase margin to help design."
->Our customer would like to have 45degrees phase margin.So, could you let us know Stability Boundary Conditions like as app note?
<Additional question2>
We could not find ESR discription for the stability on the app note.
Do you have the stability characteristic diagram with ESR vs CL(Load capacitiance - uF)?
Kind regards,
Hirtotaka Matsumoto
Michael san
And then, our customer would like to simulation to confirm phase margin using TINA-TI.
We sent you files using private message.(Because this design inculdes confidential(customer's circuit) content.)
So, could you give us the some advice?
We need your help.
Kind regards,
Hirotaka Matsumoto
Michael san and team
We are sorry to rush you, however could you let us the advice?
Kind regards,
Hirotaka Matsumoto
Hello Matsumoto-san,
1) Unfortunately, we do not have the bode plot data to show for 45degrees phase margin. To maximize the margin while having capacitance on the cathode, I suggest >10uF of capacitance, and the more the better.
2) I am not sure i understand the question. Are you looking for an additional ESR graph that shows 45degrees phase margin? All the data that we have provided in Figures 5-8 in the application note is what we have. http://www.ti.com/lit/an/slva482a/slva482a.pdf
The additional ESR will help with stability, but knowing exactly what the phase margin will be would require a bench test.
Best,
Michael