Part Number: TL431A
I am currently working on a universal solar charger eletronic circuit which I bumped into on the internet. In the circuit we do have a shunt zener diode tl431a. I need to modify the circuit to that of an led lamp driver but the problem that I do have is that the supply is dc 12 volts @ 75 amps and the other option is that I can use 12 volts @ 68 amps but my fear is on the zener shunt diode incase it may blow.If you can assist me with the modifications I can make to see to it that it does not blow up the circuit. I have also attached the circuit diagram for the universal charger. I intend to power up to 12 led lamp drivers rated at 22 watts or 32 watts.
Please if you can help me out I am stuck.
Regards
Bernard TendenguUNIVERSAL SOLAR CHARGER.pdf