Hello.
I am interested in a very precise voltage pulse generator that will be used as a verification system.
Basically, I would like to generate a pulse with an integrated voltage of approximately 0.1 Vs. Most importantly, I need to have the precision (repeatability ) of the integrated voltage from this pulse better than 1e-5 Vs. Both the time interval and the amplitude of the signal should be very precise. I am not concerned with the amplitude of the signal. A 10 V x 0.01 s pulse or a 2.5 V x 0.04 s (both examples have 0.1 Vs) will be fine.
Additional information:
- The device that will read the pulse signal is a NI module (PXI 4464);
- The pulse generator will be in a closed environment, with controlled temperature and humidity.
- Since we have space constraints, we are looking for small devices/components to provide the pulse.
I was wondering if someone could recommend me devices and/or components in order to achieve our goals.
The LM4132 seems to be appropriate for my application. But I am not familiar about which additional components I should include in order to make it works.
Regards.