In the recommended operating conditions, it shows output voltage should be 1.24 to 10V.
Does this mean when the part is active? For example, if I have this circuit:
If the input voltage ramps up to 22V, the circuit kicks in at ~18V. After the LM4041 is conducting the voltage will be be ~2V which is OK for the part. Before the part turns on it would exceed the max recommended output voltage. Is this an issue??
Thanks