Part Number: LM4040B
The recommended range is -40 to 85 degrees. I would like to know the impact of operating closer to an ambient temperature of -55 for a short period of time (<2 hours) Is the risk that the component will fail or will the operating parameters be wider than is normally acceptable? I'm having the same issue with the LM2901M which appears to be tested at -55 but is rated at -40.