Hi,
Could you tell me about Vout accuracy.
When thinking about the worst case of accuracy of Vout taking temperature into consideration,
I understand that it is enough to add "output voltage temperature drift" and "Thermal hysteresis" in consideration of "initial accuracy",
is it correct?
For example, if you want to calculate Vout at 80 ° C environment,
if I consider the worst case, can I calculate by adding ± 0.15% to 1.25 V plus the calculation results of "Output voltage temperature drift" and "Thermal hysteresis"?
Best Regards,
Yuto Sakai