Other Parts Discussed in Thread: TL431, LM4041-N, LM4040
Hi,
I want to use the ATL431 for a 4V reference, and from the datasheet Fig 14 and 15 it seems that there will be some cases where it will be unstable.
The cathode current should be between 0.1mA and 5mA, excluding the start-up where it could have a peak up to 100mA.
To overcame the instability problems, as suggested. I am planning on using a very high capacitance.
Do you think 4 x 47uF will be enough?
Do you have some graphs that will show the stability for C > 10uF, and possibly 4V reference? (something like slva482a that is for TL431)
Thankjs