This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF2125: REF2125 use Vref voltage for sequencer UCD90320

Part Number: REF2125
Other Parts Discussed in Thread: UCD90320

Hi.

I want to use a reference voltage REF2125 for the chip UCD90320.

I use REF2125 with the following connection parameters: Cin = 4,7uF, Ccs = 100nF, Rcs=330 Ом, Cout 4,7uF. At source (REF2125) out voltage = 1.9V, but should be 2,5V.

I can something that is not connected correctly?