Other Parts Discussed in Thread: TLV431
Hi,
As I'm doing both a noise sensitive and power sensitive design, I plan to run the LMV431 at considerably lower current than 1 mA. I can not find any literature specifying how noise is effected at lower than the 1mA test current. A graph of nV / Hz E -2 vs current at 1 KHz would be nice. Only reason I'm not using the TLV431 is that I plan to make the reference 16 Volts so if the divider resistors add to the noise I also need to know that.
Best regards,
Marty