Welcome to the /etc... Power Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: TL431BQDBZRQ1 Voltage Raring and Protection circuits by 752052
Questions for TL431BQDBZRQ1
Q1: What's the maxim voltage rating between Ref and Anode?Q2: Are there any protection diode or protection circuit for Ref Pin? Please let me know detail of internal circuit of Ref pinQ3: Is there any protection circuit for ESD? Is TL431 guaranteed for ESD rating? How about spec.? Q4: What's the maxim voltage rating between Cathode to Ref? Are there any protection circuit between Cathode and Ref pin?
Best regards,
Q: Re: TL431BQDBZRQ1 Voltage Raring and Protection circuits by 9125
Q1: What's the maxim voltage rating between Ref and Anode?
Answer: In forward bias, between Ref and anode are 2 PN junction in series with 3.28K and 2.4K//7.2K. It is current driven input and the absolute max forward current is 10mA. I believe voltage rating is not accurate because of these resistors tolerance. Check datasheet internal circuit.
Q2: Are there any protection diode or protection circuit for Ref Pin? Please let me know detail of internal circuit of Ref pin
Answer: In reverse bias, between Ref and anode are 2 PN junction and the absolute max reverse current is 50uA. Check datasheet internal circuit.
Q3: Is there any protection circuit for ESD? Is TL431 guaranteed for ESD rating? How about spec.?
Answer: HBM = 2.5KV, CDM = 1KV and MM = 200V. It is in the datasheet.
Q4: What's the maxim voltage rating between Cathode to Ref? Are there any protection circuit between Cathode and Ref pin?
Answer: between Cathode and Ref is NP junction (collector to base of bipolar transistor). I believe the breakdown is 37V like Cathode to Anode.
Regards, Mahmoud