Hello TI experts,
I use a 17S BMS board with two BQ76930, the 1st for 1 to 8 (from gnd), and the 2nd for cells 9 to 17. The 2nd is supplied with an isolated DC/DC and have an I2C isolator to communicate with the MCU which is referenced on pack GND.
Everything works well, but I have some questions and a curious behavior.
Question 1 :
For the temperature reading we must firstly calculate the voltage at TSx pin and then calculate the resitor value of the sensor.
The datasheet gives this formula page 25 :
VTSx = (ADC in Decimal) x 382 μV/LSB
RTS = (10,000 × VTSX) ÷ (3.3 – VTSX)
But from the internal chip diagram, the ADC for temperature is the same for cell voltage measurement.
Thus I think we should also use the Gain and Offset of the chip to calculate VTSx, as for cell voltage ?
Question 2 :
What is the precision of the 3.3V regulator applied to the internal 10K and external thermistor for the temperature measurement ?
Question 3 :
In my software in the main loop I pull the CC_READY bit in the SYS_STAT register for the 2 chips, and when the bit is 1, I read all data register to get cell voltage and temperature. For debug I flash a different led for each chip when data are ready, and I can clearly see the "phase" changing on led flashes. It clearly indicates that the 250ms sample interval are not exactly the same between the 2 chips.
What is the precision or tolerance for this 250ms timing ? The datasheet doesn't talk about this.
It can be a problem because my MCU calculate the ampere-hour outgoing of the pack based on this timing. The Ah calculation will be wrong if the 250ms is not precise.
Curious behavior :
I use a serial port of my MCU to output debug message, and when I display the cells voltage measurements (each time CC_READY is 1 thus at 4Hz rate), I can see sometime a deviation of the value on some cell. More precisely on the upper cell of the internal five cell group (VC5 and VC10). There is nothing connected on the battery pack (no charge, no discharge, thus zero current). It's the same behavior for the 2 bq76930 of the board, for example, for the low side bq76930 (cell 1 to 8), incorrect values are in bold :
BQ 0 : 3749mV 3749mV 3750mV 0000mV 3740mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3749mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3743mV 3745mV 3747mV 3747mV 0000mV 3724mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3747mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3751mV 0000mV 3748mV 3745mV 3749mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3749mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3724mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3743mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3749mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3724mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3742mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3721mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3742mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3744mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3724mV
BQ 0 : 3749mV 3750mV 3751mV 0000mV 3742mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3741mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3749mV 3747mV 0000mV 3723mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3743mV 3745mV 3749mV 3746mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3748mV 3746mV 3746mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3724mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3743mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3724mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3742mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3724mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3743mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3724mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3743mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3751mV 0000mV 3748mV 3745mV 3747mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3749mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3721mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3747mV 0000mV 3742mV
BQ 0 : 3750mV 3750mV 3751mV 0000mV 3743mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3749mV 3747mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3751mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
BQ 0 : 3749mV 3750mV 3750mV 0000mV 3748mV 3745mV 3748mV 3746mV 0000mV 3742mV
Same thing with the high side bq76930 (cell 9 to 17) :
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3739mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3738mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3720mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3739mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3744mV 3744mV 3745mV 3743mV 3739mV 3743mV 3743mV 0000mV 3739mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3720mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3744mV 3740mV 3743mV 3743mV 0000mV 3737mV
BQ 1 : 3742mV 3743mV 3743mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3738mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3742mV 3743mV 0000mV 3720mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3739mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3739mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3743mV 0000mV 3739mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3738mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3743mV 0000mV 3719mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3743mV 0000mV 3719mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3744mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3739mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3743mV 3736mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3743mV 0000mV 3720mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3739mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3739mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3738mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3741mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3718mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3741mV 3743mV 3743mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3739mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3739mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3720mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3744mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3739mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3744mV 3740mV 3741mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3745mV 3743mV 3740mV 3744mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3744mV 0000mV 3719mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3744mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3739mV 3740mV 3743mV 3743mV 0000mV 3739mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3739mV 3743mV 3744mV 0000mV 3739mV
BQ 1 : 3742mV 3744mV 3744mV 3745mV 3744mV 3739mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3745mV 3743mV 3739mV 3743mV 3743mV 0000mV 3720mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3739mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3745mV 3744mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3744mV 3744mV 3745mV 3737mV 3740mV 3743mV 3743mV 0000mV 3737mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3743mV 3743mV 0000mV 3720mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3739mV
BQ 1 : 3742mV 3743mV 3743mV 3745mV 3743mV 3740mV 3743mV 3744mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3738mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3743mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3720mV
BQ 1 : 3741mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3744mV 3740mV 3743mV 3744mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3738mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3742mV 3740mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3742mV 3743mV 0000mV 3720mV
BQ 1 : 3742mV 3743mV 3744mV 3744mV 3743mV 3740mV 3743mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3744mV 3740mV 3742mV 3743mV 0000mV 3738mV
BQ 1 : 3742mV 3743mV 3744mV 3745mV 3743mV 3740mV 3743mV 3743mV 0000mV 3739mV
Please note that's really a measure problem and not a communication error because I use a bq76930 with CRC option, and the CRC validation is implemented in my firmware. All data registers are read in a single contiguous read with auto increment. And all balancing are OFF.
Any idea for this ~20mV periodic deviation for VC10 and the ~5mV periodic deviation for VC5 ?
Regards
Cyril HAENEL