BQ25898 follows JEITA profile, and change charging current by different temperature.
for example, in datasheet, pp.11, V(T2), T2 (10°C) threshold, charge back to ICHG/2 (REG04[6:0]) and VREG (REG06[7:2]) below this temperature.
the question is: does the change apply to IPRECHG as well?
assume IPRECHG is set to 256mA, will the current be 50mA with REG07[0] =1 at 10°C
thanks