This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LM25141: What happened if the Vin and Vout of the LM25242 are short-circuited?

Part Number: LM25141

Hi all

     I set the LM25141 output is 12V, and Vin is 24V. If the misoperation, the output is shorted to Vin, what happened to  the LM25141 ? Will it be burned ? or be auto protection ?

    Thanks a lot.

  • Hi Went,

    Let me get back to you on this one

    Thanks
    -Arief
  • In reply to Arief Hernadi:

    Hi went,

    The part will get damaged because VOUT pin abs max rating is 15.5V

    Thanks
    -Arief

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.