Tool/software: WEBENCH® Design Tools
Hi,
i like the TPS2491 Power Limiting feature, because sometime Current limit is not enough protection.
i would like to use the TPS2491 in a 1275D/E Surge protection.
the 1275 standard requires accomodating with +/-7V around the 28V, frequency 50Hz-200KHz
my question is : does the TPS2491 knows to handle also this "AC" signal. becuase the data sheet assumes all voltages are DC.
What is the response/behavior of the TPS2491 under Voltage Input with Quite high ripple ?
thanks
amos