Other Parts Discussed in Thread: TINA-TI, LM5114
I need very fast capacitive load driver for 60MHz pulse ( duty: 50% ) with 1nF Capacitive Load and very low Rise/Fall/Propagation Delay.
I Think LMG1020 is the closest solution for fast driving.
However 5Vdd power supply is little higher value that I need.
My Ideal requirement Vout is 0 to 4V but I think it is too low to use lmg1020 driver.
Can I use LMG1020 with 4.5V supply? ( I know 4.75 V is minimum but TINA-TI simulation is OK with 4.5V dc supply)
If it is impossible I want to use simple mosfet inverter (buffer) to change voltage swing level with very fast response time
Could you recommend CMOS pair applicable 60MHz 4V pulse? or Other solutions for nanosecond pulse capacitive load driver?
Thank you.