This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160: lm5160 evm question

Part Number: LM5160

hi customer design requirement

3W

1.

Vin=12V~24V(Linear mode)

Vout=5V(isolate)

2.

Vin=12V~24V(Linear mode)

Vout=3.3V(isolate)

3.

Vin=12V~24V(Linear mode)

Vout=±15V(isolate)

is LM5160 a suitable solution?

which one of the EVM is better for testing?

 

LM5160DNTBKEVM Wide Input 65V, 1.5A Synchronous Step-Down DC-DC Converter

http://www.ti.com/tool/LM5160DNTBKEVM?keyMatch=lm5160&tisearch=Search-EN-Everything

 

LM5160DNTFBKEVM Fly-Buck Isolated Bias Supply Evaluation Board

http://www.ti.com/tool/LM5160DNTFBKEVM?keyMatch=lm5160&tisearch=Search-EN-Everything