• TI thinks resolved

LMG3410: usage of the device in full bridge to generate +400V to -70V drive

Part Number: LMG3410

After reading advance info/datasheet  and some details, I  was wandering if this device can be used in full bridge mode to generate +400V /-70V  drive --- Yes I am interested in  in positive 400V and negative  70V .

I am thinking about driving capacitive load of about 450nF  up to 400hz  in sinusoidal drive...

Are there any limitations ? 

Can we use the same device to generate 400V /-70V as well ?

is there a way to configure it to make it work in like class D amplifier  to save power ?

K B Shah