Hi,
we are currently working on a DC/DC Converter witch should be able to work in either Buck or Boost mode. The DC/DC converter has two Low Side and two High Side GaN FET's (EPC2021) in parallel per half bridge. During the first startup of the DC/DC converter we encounter a problem with the charge pump of the LM5113. In the first scope below you can see the HS node in green and the HB node in blue. The settings for our converter was buck mode with a dutycycle of 25%.
We expected to see that the HB node voltage rises when the Low Side ist turned on but instead we see no rise of the HB node voltage. The first 3-4 flanks of the High side look good but then we see an very slow falling edge (on the second scope). In scope 3 we can observe the behaviour of the voltage on the HB node rises after about 15-20ms. From there on the DC/DC converter works well.
Have you seen such a problem before? Any advice?