I'm looking for an application circuit which will allow me to pulse the drain supply to a GaN FET.
The circuit needs to switch between 0V & up to +50V, handle currents of up to 5A, at speeds up to 2MHz with a duty cycle which may go down to 10%.
The current solution uses a LTC4444 High Voltage Synchronous N-Channel MOSFET Driver driving a high side & low side switch, but I was interested if the Texas Instruments LMG3410 or LMG5200 may be suitable for this type of application & if so how best to use them?