Other Parts Discussed in Thread: TINA-TI, , TIDA-00909
I want to use this module to boost 30v to 48v at loads up to 100W.
This seems to provide several challenges.
First of all there is the question of overshoot. In a slight adaptation of the reference TINA-TI schematic, voltage spikes of close to 100V were seen. What can be done to reduce/eliminate those? As I understand, 100v is the maximum allowed for less than 2% of the duty cycle. One thing I'm looking into is soft-switching, which is not trivial.
The other issue is that the grounds should not be connected externally. But with multiple phases, a loop is created through the internal ground connection of the other modules. How big of a problem is this, and how can it be dealt with?