This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53632G: I2C

Part Number: TPS53632G
Other Parts Discussed in Thread: LMG5200, , LM5141

Hello,

I am planning to build a GaN FET based buck converter 24V to 5V @ 1A Max. Can I use any other TI’s synchronous buck controller (1MHz switching) to drive LMG5200? I don’t want to use I2C control to program output voltage to keep it very simple. Solution for LMG5200 half bridge GaN makes use of TPS53632g and needs to be configured/set through I2C

Regards,

Shailendra