Part Number: LMG5200EVM-01A
My team needs an amplifier capable of 50V (1A max) @ 7MHz to provide wireless power/data through resonant coupled coils. We liked the look of your LMG5200 and bought a handful of the LMG5200EVM-01A eval boards. By bypassing the inductor and removing the capacitors at the SW output we had what seemed like a workable Class D amplifier. These modified boards were providing plenty of power and producing a useful signal over the coils (despite what looks like some 100MHz noise) but a few of them have failed after moderate use.
It is unclear to us whether these failures are due to something like racethrough current, or if we are just outside the operating frequency. A search through the Community forums suggests that these boards are rated for 5MHz, but that they should be able to operate at a higher frequency than that.
So my real question is: does TI have a better product for our requirements than the LMG5200?
Thanks in advance.
Adam