Working in a University lab. Is using LM5113 DSBGA recently. Get the PCB and find the solder mask is not as good aligned as expected. Some pads are large while others are small.
I tin the pins and use hot air to solder (typically doing these in university lab). Check the pins connection and find some of them are not connected, try 10 times unluckily none working. Is there any suggestions that I can still use these PCB without getting a new layout. The boards are still under IPC class 2 tolerance.
Have some Questions:
Q1: Is that going to save the board If I order a laser cut stencils and use type 3 solder paste.
Q2: Is LM5113 DSBGA has to use laser direct imaged solder mask?