Other Parts Discussed in Thread: , TIDA-00909
Hi,
I want to operate LMG5200 at 1+Mhz frequency range.
The PWM signals are generated from a microcontroller (3.3V).
What all are the considerations i need to check before connecting it to the HI/LI pin of module.
What value of series/termination resistor should i be using while interfacing.
It would be helpful if you can post a sample circuit for the same.