Can I use a ferrite bead in series to the 5V VDD supply to LM5113 in order to reduce the EMI coming from switching? The frequency I am working on is 6.78MHz. VDD is 5V and I am driving EPC2019 (two of them in differential mode). Here, I am concerning about the EMI on the VDD line of LM5113, even though it is far less than the EMI coming from the switching of EPC2019. The ferrite bead I want to use is MH1608-601Y which can pass 1A current and has a DCR of 0.2 ohms.