Hi Team,
A customer would like to know the difference between the LMG5200EVM-01A and the LMG5200EVM-02? As far as I can see, they are the same and I couldn't find any differences.
Regards,
Mihir Gupta
FAE - South Germany
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
A customer would like to know the difference between the LMG5200EVM-01A and the LMG5200EVM-02? As far as I can see, they are the same and I couldn't find any differences.
Regards,
Mihir Gupta
FAE - South Germany
Hi Mihir,
Thanks for you interest and that is a good question.
A part from some minor improvements to the layout, the major changes are :
1. the half-bridge stage installed on the -01A part is the PLMG5200 (pre-release) instead of the LMG5200 (fully released) on the -02
2. the output capacitors have been changed to have a rating of 100V on -02 up from 25V on the -01A board.
For the rest the boards are effectively the same.
Best regards,
Alberto