• TI thinks resolved

LMG5200: Looking for similar working at 400V

Part Number: LMG5200

Hi, I am looking for a driver that would allow me to drive two GaN FET at 400V from 4MHz to 10MHz or better a solution similar to LMG5200 at 400V instead of 80V. (and no I don't plan on using 5 LMG5200 ;-) )

Two LMG3410 could help but if I am not wrong it works only up to 1MHz. 

Greetings,

Stephane