Other Parts Discussed in Thread: SN74LVC1G08, TIDA-01573
Hello support team,
I have question about test setup for the TIDA-01573.
In the description of page-11, 3.2.1 Test Setup, the input signal range for J3 is mentioned 0V to 3V. But, its input device SN74LVC1G08 is used with VCC=5V, therefor the input VIH(min) is 5 x 0.7 = 3.5V.
I think the function generator input range should be 0V to 5V. Is my understanding correct?
Best regards,
Kaizawa