Other Parts Discussed in Thread: LMG1205,
Hello Team,
One of my customers is looking to use the LMG1205 in a 100% duty cycle application. They also have ~100uA of gate to source leakage on the top side driver output. The engineer would like to pull HB up to an 8V source through a current limiting resistor to keep HB charged to 5V. However, I don’t have specifications on the 5V clamp inside the LMG1205, so I can’t determine how much current the clamp can support while maintaining regulation. Are there any details of that clamp you can share we met so I can advice the engineer?
Ideally they woud just drive HB with low impedance 5V themselves, but they are worried the clamp could be under 5V and thus burn lots of power.
Block diagram below.
Thanks,