I could not use the LMG 5200.
I think that I will write the reason first.
Only voltage of 2 V to 3 V can be applied between VCC pin and AGND.
Current flows from 1A to about 2A, between the pins.
That's why I believe it is short-circuited. But I do not know why such a thing happened.
So I will describe everything that I did.
I applied cream solder to each metal part of the backside terminal.
And the metal feet were attached to the metal parts of each terminal.
It is now possible to enter signals.
A 0.1 μF laminated ceramic capacitor was soldered between the VCC pin and the AGND pin and between the HS pin and the HB pin.
I input a 3 V pulse signal to the HI and LI pins using the FPGA.
A pulse signal with a period of 50 us was input to the HI pin.
Next, the pulse signal input to the HI pin is inverted, and a 48 μs pulse signal with 1 us set as the dead time is input to the LI pin.
5 V was applied from the voltage source between VCC pin and AGND pin.
Next, 15 V was applied from the voltage source between the VIN pin and the PGND pin.
And 5 V could not be applied between VCC pin and AGND pin.
As I wrote in the beginning, the voltage can only be applied from 2 V to 3 V, and the current will increase from 1A to about 2A.
This is turning the current pin, no voltage can be applied, only the current is applied.
Since I use half-bridge GaN like CMOS, I wanted to try first if LMG 5200 could be used.
However, it was impossible to apply a voltage between the VCC pin and the AGND pin in the first place, and the LMG 5200 could not operate.
I am very thankful if you will help me.