I was wondering what the mounting type was on this. is it a surface mount or is it a through hole? My team needs a through hole mounting to run tests on a breadboard. Does one exist for the LMG1020?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rocky,
The LMG1020 is in a WCSP package.
You have two options for your prototypes:
1. Try to find an adapter board to solder the LMG1020 on, that has pins. You would still need a hot air soldering station for this.
2. Use the EVM for your project.
This part is designed for very high frequency applications. Stray inductance is your enemy, so any leaded structure will force you to reduce your operating frequency. You really need a dedicated PCB designed to accept the WCSP package with a small loop inductance to your power devices. See the EVM for an example.
Let us know if you have further questions!