This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

17.0V to 15.0V isolated and non-isolated power supply

Hi all,

From 17.0V DC supply I need to generate 15.0V at 500mA isolated power supply and 15.0V at 500mA non-isolated power supply both. I tried with WEBENCH Designer, but wasn't convinced with designs. Please suggest a TI/National  part number with schematics if possible. Please refer the power supply tree below for clear reference.

Thanks and regards

-Anand

  • In the future, I would recommend making this two separate posts since you want two very different power supplies.  I moved this to the isolated forum, where they can help you choose a controller for your isolated need.  A flyback would likely be the best option.

    For the non-isolated power supply, an LDO would be simplest.  The TPS7A4801, TPS7A4501, and TPS73801 all look like options.

    Chris Glaser

    Texas Instruments

  • Anand,

     

    On th eassumption that the 17 volts might drop I would recommend the UCC38C45

    http://www.ti.com/lit/ds/symlink/ucc38c45.pdf 

    It is a flyback design and should be fairly simple to implement. With a 50% limitation on the duty cycle you should not have to implement slope compensation.

    A resonable app note to review for your design is http://www.ti.com/lit/an/slua274a/slua274a.pdf 

    Since you are powering this from a 17 volt source you should be able to power it through a simple series regulator that results with VDD at 9 volts.

    Regards,

    John 

     

    John Bottrill

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.