• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » AC/DC and Isolated DC/DC Power » AC/DC and Isolated DC/DC Power Forum » TPS40210 configured as isolated forward
Share
AC/DC and Isolated DC/DC Power
  • Forum
Options
  • Subscribe via RSS

Forums

TPS40210 configured as isolated forward

This question is not answered
mod13192
Posted by mod13192
on Jul 08 2009 21:44 PM
Prodigy90 points

Hi,

I want to use TPS40210 as an isolated forward converter. (I want to minimise o/p ripple)

Can i configure it this way? How would the feedback be?

My requirement is 9 to 36V input; output is 5.1V 1.4A

Thanks.

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • nancy!
    Posted by nancy!
    on Jul 10 2009 10:57 AM
    Intellectual2765 points

    Hi Mod,

    The TPS40210 can be operated as an isolated forward converter, however the internal error amplifier will make the feedback process a little tricky. 

    Typically in an isolated design customers use a TL431 shunt regualtor and opt-coupler to pass outvoltage and frequency compensation across the isolation barrier. 

    Page 10 of the Third Quarter 2008 edition of TI's Analog Applications Journal (http://focus.ti.com/lit/an/slyt297/slyt297.pdf) shows the schematic for the TPS40210 in an isolated flyback configuration, but the isolated feedback scheme is the same.

    The TL431 on the secondary side performs the reference comparison and loop compensation.  An opt--coupler passes the resulting control information across the isolation barrier and the TPS40210's error amplfiier drives the control voltage (COMP) to generate the required PWM signals.

    Regards,

    Nancy

    It is not the strongest of the species that survives, nor the most intelligent that survives.  It is the one that is the most adaptable to change. - Charles Darwin

    TPS40210
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • mod13192
    Posted by mod13192
    on Jul 10 2009 22:01 PM
    Prodigy90 points

    Thanks Nancy...

    I already did it on my PCB layout... waiting for the sample IC to arrive

    I still have some questions.

    What is the practical reset ckt for the transformer? (I implimented RCD on my layout but consumes a lot of space). Is a resonant reset applicable?

    If i will not add a reset ckt,  it probably not destroy the MOSFET switch (i will use 100V) but will the transformer saturate? Switching frequency is 400KHz.

    What is the maximum allowable duty cycle at the lowest input voltage?

    Regards,

    mod

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Peter Miller13277
    Posted by Peter Miller13277
    on Jul 13 2009 11:57 AM
    Genius16505 points

    I already did it on my PCB layout... waiting for the sample IC to arrive

    I still have some questions.

    What is the practical reset ckt for the transformer? (I implimented RCD on my layout but consumes a lot of space). Is a resonant reset applicable?

    RCD will offer several advantages for reset.  It is more efficient than rosonant reset, produces cleaner waveforms and allows higher duty cycles.  Resonant reset has lower efficient, applies more voltage stress to the switching FET (typically upto 2x the input voltage) and can have issue above 50% duty cycle.

    If i will not add a reset ckt,  it probably not destroy the MOSFET switch (i will use 100V) but will the transformer saturate? Switching frequency is 400KHz.

    If the duty cycle doesn't exceed 50% you shouldn't have a problem with saturation using resonant reset.  At higher duty cycles resonant reset can have reset issues with the transform's V-s becoming unbalanced.  Without a synchronization circuit, there is no effective way to limit the maximum duty cycle of the TPS40210

    What is the maximum allowable duty cycle at the lowest input voltage?

    For the IC's limitation, at low-line, the controller can operate upto 95% duty cycle, however this would likely damage a forward converter with transformer saturation.  In practical terms, you should adjust the transformer turns ratio to make sure the converter is always less than 50% duty cycle to provide for transformer reset. 

    The only way to effectively Duty Cycle Clamp the TPS40210 is to pull the RC pin above Vin / 20 during the unused portion of the duty cycle.  (Applying a 60% duty cycle pull-up on the Vin pin via a diode pull-up effectively synchronizes the TPS40210 to the falling edge of the external signal and limits the duty cycle to 40% (1-D of the synchronization signal)

    Peter James Miller

    IC Design

    Power Management - DC/DC Solutions - Industrial & Communications DC Solutions

    Member Group Technical Staff 2008

    TPS40210 Forward Duty-Cycle Clamp
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • mod13192
    Posted by mod13192
    on Jul 19 2009 20:47 PM
    Prodigy90 points

    Hi Peter,

    Thanks for the clarifications.

    Unfortunately, samples ICs will not be available 'til next month.

    For the mean time, could you send the link for simulation software using a/m IC configured as forward converter. The one on your web is for boost.

    Thanks again and more power.

    Cheers!

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Peter Miller13277
    Posted by Peter Miller13277
    on Jul 20 2009 08:43 AM
    Genius16505 points

    Mod,

    There is no forward converter simulations tool currently available for the TPS40210 controllser.

    Peter James Miller

    IC Design

    Power Management - DC/DC Solutions - Industrial & Communications DC Solutions

    Member Group Technical Staff 2008

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • mod13192
    Posted by mod13192
    on Jul 26 2009 23:40 PM
    Prodigy90 points

    Hi Peter,

    I am now doing the initial test of TPS40210, evrything seems fine except for the UVLO trigger point.

    It starts operating at 4.7Vin (there is unbalanced V-S), when it reaches 5.4V the OCP kicks off making it re-start. At the time Vin is 6.1V the output is already regulated but the transfomer is not resetting properly. 

    Is there any way that i could adjust it to around 8V with hysteresis of 0.5V?

    Thanks.

    UVLO
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Peter Miller13277
    Posted by Peter Miller13277
    on Jul 27 2009 11:26 AM
    Genius16505 points

    The TPS40210 controller does not include a programmable UVLO function, so you'll need to build an external UVLO function using the IC's Disable Pin.

    The Disable Pin has an internal pull-down, so the pin must be externally pulled-up to be disabled.  Pulling this pin low will turn the IC on.  Unfortunately this isn't going to be a trival circuit and the design will depend on what other rails may be available in the circuit at the time.

    You can build a very "rough" (loose tolerance) UVLO with a resistor divider and an N-channel MOSFET.  A diode, resistor and capacitor from the gate driver can feed additional current into the divider to provide hysteresis.  For more accuracy, you'll have to go to a comparator to drive the N-channel MOSFET or the disable pin directly.  Again, a diode from the gate to a capacitor (peak detector) with a resistor to the junction point of the resistor divider for the UVLO sensing will provide hysteresis by providing additional current once the TPS40210 converter starts switching.

    NOTE: The BP regulator is disaled when the disable pin is pulled high (IC disabled) so this pin can not power the UVLO circuitry.

    Peter James Miller

    IC Design

    Power Management - DC/DC Solutions - Industrial & Communications DC Solutions

    Member Group Technical Staff 2008

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • mod13192
    Posted by mod13192
    on Jul 30 2009 21:40 PM
    Prodigy90 points

    Hi Peter,

    I just build a UVLO with a loose tolerance as u satated, but instead of adding a peak detector ckt from the gate driver i used the BP pin with a 680K resistor to the junction of the resistor divider.

    It works fine now.

    Your forum is a great help... keep it up

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Peter Miller13277
    Posted by Peter Miller13277
    on Jul 31 2009 09:27 AM
    Genius16505 points

    One caution on using the BP voltage for UVLO hysteresis.  The hysteresis on turn-off will be much lower as it takes a long time for the BP regulator voltage to discharge in shutdown.  To see if this could be a problem in your circuit, run the converter under full load and then provide the slowest Vin power down profile you expect.  The concern is that during power down when the converter reaches UVLO_off and load on the source is removed the input voltage will increase sufficiently to turn the converter back on.  Since BP has not discharged the hysteresis going from UVLO_OFF to UVLO_ON will be fairly low.

    Using the peak-detector improves the UVLO in this case by using a much smaller capacitor than the BP regulator to allow this voltage to discharge much more quickly.

    Peter James Miller

    IC Design

    Power Management - DC/DC Solutions - Industrial & Communications DC Solutions

    Member Group Technical Staff 2008

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • mod13192
    Posted by mod13192
    on Jul 31 2009 23:13 PM
    Prodigy90 points

    I will check it out when i get back to work on monday.  I also reduced the cap on BP pin from 1uF to 0.47uF

    One concern i have is the o/p line ripple when Vin is greater than 26V and load current is at minimum(50mA). The converter seems to reach its minimum duty cycle and it is cycle skipping ,creating a line ripple of about 50mVpp. I tried to play around the compensation values, and turns ratio of the transformer but may attempts failed. Though the ripple has a relatively low amplitude, it is to me an unstabilty of the power supply. Pls enlighten...

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Peter Miller13277
    Posted by Peter Miller13277
    on Aug 11 2009 14:48 PM
    Genius16505 points

    Mod,

    If you are operating below the minimum pulsewidth of the controller, the switching frequency will be less than that of the internal oscillator, which would force evaluating the stability of the converter at 1/2 or less of the switching frequency.  In addition, the change in switching frequency changes the loop characteristics of the modulator, drastically changing the total loop response which could be resulting in unstable operation.

    With only 50mV of output ripple, it is more likely that the ripple is a result of overshoot from a minimum pulse width followed by missing cycles waiting for the output voltage to fall back to the internal reference.  What looks like a low-frequency stability issue may be the beat frequency between the fixed frequency internal clock and the natural hysteretic response of the L-C running at minimum on-time.

    Peter James Miller

    IC Design

    Power Management - DC/DC Solutions - Industrial & Communications DC Solutions

    Member Group Technical Staff 2008

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use