Converter Requirements:
Vac: 80-265V
Vout: 390V
Pout: 1400W
PF: >0.99 at rated load
Architecture: 2-phase Interleave
Controller: TI UCC28070
Design Details:
Boost Inductor: 160uH-->260uH
Voltage Loop BW: 7.5Hz, PM=52 deg calculated
Current Loop BW: Changed from 23KHz, PM = 52 deg to 10Khz, PM=40 deg
Cbulk: 492uF
Problem Description:
PFC converter becaomes unstable at full load when Vacin is slowly decreased across QVFF boundaries, particularly at low lines, <120Vac. The disturbance is recoverable at light to mid load but is irrecoverable at full load.
Steps Required to Recreate Problem:
Set Pout=1400W, Decrease Vacin gradually from 135Vac to 75Vac. Three QVFF boundaries will be encountered. At each boundary the perturbation can be observed on the oscilloscope. At some boundaries, particularly the lowest two, the converter will break into an irrecoverable unstable state. The symptom is recoverable at Pout of 1000W and lower.
Discussion:
When converter entered the "unstable" state, it seems the controller is transitioning between QVFF states, ie insufficient input voltage hystereis. During the symptom, all UCC28070 control signals are behaving "true to form".
Question:
Has anyone encountered a similar problem with this controller and how was it resolved?