This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3.5kW PFC without input Rectifier Bridge, using UCC28070

Subject:  PFC--3.5kW using UCC28070 Interleaved input Bridge & Bridgeless

kindly send me the excel design tool for PFC using UCC28070.

i already have " UCC28070 Design tool 8 15 08 " ---but this is with a single controller.

i want the design tool using 2 nos. of controllers with 180 deg. phase shifted. + i want the design tool using 2 nos. of controllers with 180 deg. phase shifted for a BRIDGELESS PFC  design.

Rajesham.E.

Triport Energy Systems

93472 56728 / 9140 2794 0197